Part Number: CDCE925
Hi
When the external clock is provided using the clock buffer, the frequency cannot be adjusted; It can be adjusted when using the crystal directly as an external clock source.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCE925
Hi
When the external clock is provided using the clock buffer, the frequency cannot be adjusted; It can be adjusted when using the crystal directly as an external clock source.

Hello,
Are you trying to use the part in VCXO mode, in XTAL mode, or in LVCMOS clock mode for the input buffer? If in VCXO mode, this will not work without an XTAL input.
Can you please provide the configuration that is being used for both conditions?
Thanks,
Kadeem
Hi Kadeem,
They can not adjusted output frequency when input is clock buffer in LVCMOS mode. Is there any other reason.
Hello,
Is the series output resistor required by the 8L30110 clock buffer present?
Is the clock present and register changes are not changing the output frequency? If they write and read back, are the registers the same as the written values (in other words, is the device recognizing the I2C writes)?
Is the pass-through path for Y1 able to output a 24 MHz LVCMOS clock when Pdiv1 is set to 1?
Thanks,
Kadeem
Hi,
The input is LVCMOS signal, dose it can adjust by VCXO. Customer's issue is that they can not use VCXO adjust output frequency if the input come from clock buffer LVCMOS signal.
Do you have a solution to solve problem if can not use VCXO at LVCMOS input.
The problem as below,
The input 24Mhz clock is also mcu clock input, so the VCXO need have no influence for mcu clock. MCU need clock first power on for CDCE I2C set, so mcu can not use the CDCE925 output for clock input.
Hello,
If using an LVCMOS clock input, the VCXO input adjustment is not valid. The VCXO works by adjusting the internal capacitive loading on the external XTAL to tune the XTAL. If there is no XTAL, no tuning can occur. Modification of the output frequency with an LVCMOS clock is only achievable by adjusting the PLL and divider settings.
Thanks,
Kadeem
Hi,
Do you have advice if customer need XTAL to VCXO and the MCU clock is not affected.
The input 24Mhz clock is also mcu clock input, so the VCXO need have no influence for mcu clock. MCU need clock first power on for CDCE I2C set, so mcu can not use the CDCE925 output for clock input.
Hello,
If the VCXO mode is being used, then changing the XTAL frequency will affect all clocks output by the device, including the clock used for the MCU.
A dedicated oscillator, such as the LKM6C, would be required for the MCU, with the CDCE925 generating the remaining clocks.
Thanks,
Kadeem