This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX1204: LMX1204 Equivalent Chip with Two CLKINs

Part Number: LMX1204


Hello TI Team,

I have requirement to Clock Buffer (same as LMX1204 or equivalent) for distribution of Clock frequency upto 12GHz along with JESD204B Sysref generation.

But I need two (CLKIN) inputs and internal switching option between that two inputs.

Can you suggest any other Equivalent clock buffer chip with two CLKIN inputs & all LMX1204 Functions?

Thanks in advance,

Sakthi

  • Hello Sakthi,

    In our current portfolio and roadmap, we don't have a clock buffer that can accept such high input frequencies and have two clock-ins. Why do you need 2 inputs and switch between them? What functionalities from the LMX1204 are the ones you are using? Why do you need those functionalities? If possible, it would be great to better understand your system and requirements so I could potentially suggest a multichip solution. Thanks!

    Best,

    Andrea