Part Number: LMX2594
Hi Noel,
If I change L1=18nH to 1nH,Is it effect the RF LO outpower?
| Parameter | Value | Unit |
| Fout | 15000 | MHz |
| OUTA_PWR | 50 | |
| Resistor Pull-UP | 0 | ohm |
| Inductor Pull-UP | 18 | nH |
| Load Impedance | 50 | ohm |
| R1 | 0 | ohm |
| R2 | 1E+13 | ohm |

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ray,
Yes, pull up inductor will affect RFout power.
1nH to 3nH is our typical recommendation for maximum power.
Regards,
Vicente