This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: LMK00304 as input to LMX2595

Part Number: LMX2595
Other Parts Discussed in Thread: LMK00304, , LMX2572

Hi I want to use LMK00304 as an input buffer to two numbers of  LMX2595 and to LMX2572 to feed LVDS differential Signal and i have few questions:

1) What is the maximum differential input voltage level(vOSCin)  in peak-to-peak  can be provided to LMX2595 and LMX2572?

2) Is it okay if i go with LVPECL differential input to LMX2595 and LMX2572?

Also please let me know whether the configuration i am following is correct?