Other Parts Discussed in Thread: LMX1204
The EVM used two 1 amp regulators for the LMX1204. One for the VCC01/VCC23 pins and the other for the VCC_CLKIN/VCCLOGICLK pins. The datasheet gives the typical current draw as 1050mA with everything on.
What is the max expected current draw for each one amp supply? Is the thinking that one is for digital circuits and the other analog and they need to be on separate rails?
I will be using two of the LMX1204 chips on one board and it seems like using four 1 amp regulators is overkill.
Thanks in advance.