Part Number: LMK04828
Other Parts Discussed in Thread: ADC12DJ5200RF, , LMK04832
Hi!
I am working on configuring the ADC12DJ5200RF dev board and having some difficulties programming the LMK04828B. I am using TICS Pro to configure each register with the appropriate values, then export that hex register data into our script that programs the board.
My issue is this:
The 'VCO/Clock Dist. Frequency' using VCO1 is limited between 2920 and 3080 MHz. I am constrained by what I need the clock outputs to be in order to drive and interact with peripherals, most importantly 320 MHz off one of the clocks. I cannot seem to find a configuration that maps VCO1 in the desired range and also gives me a clock output that lands clean on 320 MHz.
My question:
Is this VCO1 range absolutely firm? What exactly happens when you program the VCO1 clock outside of this range?
I tested a bunch and saw that when I configured VCO1 to 3000 MHz, all clock outputs probed cleanly and at the expected frequencies.
When I used the same configuration and just changed the input clock to 320, the VCO1 out follows to 3200. When implementing this configuration and probing, I found the clock output frequencies were all out of whack.
Looking for some insight and assistance handling this.
Thanks in advance.