Part Number: LMK04208
Other Parts Discussed in Thread: LMX2594, CODELOADER
Hello,
I am currently using TICS Pro v1.7.6.2 to configure the LMK04208 part. The application performs exceptionally well in generating the required output clock frequency.
However, I am facing a challenge when attempting to import Hex register values. The application seems to generate random values, resulting in incorrect configurations. Interestingly, when loading the TCS file, everything works flawlessly.
My objective is to inspect existing register values, make modifications, and apply them to the configuration. Unfortunately, the current bug hinders this process, making it impossible to achieve the desired outcome.
Here is the output of the TICS Pro when I import the register values:
CLKout4 must be 110 MHz but instead, it is a random value. Attached are the Register Hex Values to replicate the issue on your side.
R0 (INIT) 0x00160040 R0 0x00143400 R1 0x00143401 R2 0x00140342 R3 0x80140343 R4 0x00140344 R5 0x80141BE5 R6 0x01100006 R7 0x01100007 R8 0x06010008 R9 0x55555549 R10 0x9102410A R11 0x0401900B R12 0x1B8C006C R13 0x2302886D R14 0x0200000E R15 0x8000800F R16 0xC1550410 R24 0x00000058 R25 0x02C9C419 R26 0x8FA8001A R27 0x10001E1B R28 0x6001201C R29 0x0188BA7D R30 0x0208BA7E R31 0x003F001F
Could you kindly guide me in resolving this issue? I have attempted to upgrade to the latest TICS Pro version (v1.7.7.1), but the GUI does not function correctly.
Regards,