Part Number: LMK03328
Hello team,
Is there specific method to disable all outputs(only output buffer block) thru I2C command?

Best Regards,
Austin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Austin,
The SYNCN event can be used to disable all outputs, if the outputs being synchronized afterwards is fine.
The SYNCN_SW bit (R12[6]) controls this function.
Otherwise, the outputs can be individually powered down, or a soft chip reset can be performed (which would also result in VCO calibration).
Thanks,
Kadeem