Part Number: LMX2594
I have two questions. First, the calibration time with "no assist" is specified with a 200MHz Fosc. It appears the State Machine is based on this 200MHz. If we are using 100MHz, can we assume the calibration time will be doubled? Second, if we want to use the Phase Sync but try to use OCS_2X to increase the state machine speed and then an Rdiv of 2 to keep our PFD at 100MHz, will this still meet the requirement for keeping M=1 for phase sync? Our goal is to try to achieve the fastest calibration time while meeting the requirements for Phase Sync. Thanks!