This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208: TI clock solution recommend

Guru 12815 points

Part Number: CDCM6208
Other Parts Discussed in Thread: CDCE6214, , LMK03318

Hello,

My customer is looking for a low cost clock solution that can receive 30.72MHz TCXO output and multiply it by 2/4 to output 61.44MHz/122.88MHz as below.

    - Input : TCXO 30.72MHz

    - Output : LVDS 61.44MHz (1 port), LVCMOS 122.88MHz(1 port), LVCMOS 61.44MHz(2 port)

    - The above four outputs should be synchronized.

If there is a suitable product among TI's clock products, please recommend it.

Thank you.

JH