Part Number: LMK00334-Q1
Other Parts Discussed in Thread: LMK00334, LMK00304
LMK00334 clock buffer datasheet implied that CLKIN can support HCSL clock, however Vild_min = GND.

Most HCSL clock outputs shows Vol_min = -0.15V (including the LMK00334 - see image below).
Given this limitation, it doesn't appear that the LMK00334 can be ganged in series, or accept most HCSL clocks.
Question:
Does the LMK00334 support HCSL clock at CLKIN, if the HCSL clock has Vol_min < GND (-0.15)?