Part Number: CDCE62002
Hi,
I am currently experiencing an issue with the clock cleaner CDCE62002.
I use the clock cleaner to convert frequencies from 74.25 MHz to 74.25MHz or 148.5 MHz to 148.5 MHz. I need a perfect x1 conversion.
Most of the time, the output frequency is correct; however, sometimes it's not.
The problem arises exclusively when transitioning the input signal from one frequency to another (e.g., from 148.5M to 74.25M, or vice versa).
When the output frequency is incorrect, it's typically quite close, around 74.35 MHz / 148.55 MHz. This is not precise enough for my needs.
Below are the register values I use for converting 148.5 MHz to 148.5 MHz:
Reg0: 0x10360050
Reg1: 0x9782E061
After setting these values in the registers, I initiate a calibration by toggling PD:
Reg2: 0x01001802
Reg2: 0x01001002
Reg2: 0x01001802
Then, I wait until PLLLOCKPIN equals '1'.
The external filter has the following values: 220nF, 10R and 47uF.
The input has an AC termination.