Part Number: LMK04832
Hello,
I'm little bit confused with RESET/GPO (pin 5) functions:
1. I see in register 0x14A: the default value is 2, i.e. "input with pulldown resistor". Does it mean the default function is "RESET" and default active level is High?
2. If this pin is reprogrammed to be GPO, how reset can be provided to the LMK04832 at the runtime?
3. Is the external Power-On-Reset signal must be applied to LMK device for correct operation or may be LMK device has its own internal Power-On-Reset circuit?
Please, clarify
Thanks,
Alex