This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TICSPRO-SW: Need configuration file for LMK and LMX

Part Number: TICSPRO-SW
Other Parts Discussed in Thread: LMX2594, LMX2572

Hi,

Could someone provide me with LMK04828B and LMX2594 configuration files for the following specs?

The LMK clock out is 156.8 MHz and the reference clock to LMK is 204.8 MHz. The Sysref clk required is 7.84 MHz.

The ADC sample rate is 1.2544 GSPS.

Thank you.