Other Parts Discussed in Thread: TIDA-01410
In LMX2496, both the RF and IF have a phase detector frequency (pdf) signal divided from the oscin.
If RF_R_divider == IF_R_divider, the RF and IF parts have the same pdf, but do they have the same phase?
In the TI tech document (tidud11.pdf):
TI Designs: TIDA-01410
Phase Synchronization of Multiple PLL Synthesizers Reference Design
section 2.2.1 states:
"One thing that can cause the phase relationships to be different is if there are divides involved. For instance, whenever a signal is divide-by-two there are two possible output phases, which requires the designer to take action. "
For example, if oscin=30MHz, and RF_R_divider = IF_R_divider = 3, so both the pdf signals are 10MHz, but since they are divided by 3 from 30MHz, so they may have 3 possible phases, and the two pdf signals may not phase synchronized. Consequently, the output RF and IF signal may also not synchronized.