Other Parts Discussed in Thread: LMX2595,
Hello TI Community,
I am working on the LM2595EVM + Reference Pro with TICS Pro. My connection is exactly as shown in the diagram below (minus the 50 Ohm Termination):
Here is my TICS Pro Config File: Config File
I was successful in locking the PLL and ramping it between required frequencies yesterday (video). I come back today to work the same, but the EVM doesn't lock.
Observations:
- The Lock LED flickers on Ctrl+L / Write All Registers and goes off less than a second later
- Current draw is steady at around 172mA (before and after write)
- On Reading Registers, most registers are filled with 1s
- Sometimes on toggling the OUTA_PD / OUTB_PD, the lock LED turns on but the output doesn't show any locking
Here is what I have tried:
- Directly use the saved TCS file: Doesn't work
- Recreate the entire configuration from scratch: Doesn't work
- Clock Verification: I am getting a stable 100 MHz clock from the Reference Pro
- Remove Load: Doesn't lock
- Try Default Config and Test Mode: Doesn't work / lock
- Disconnect and reconnect everything: Performed twice, still doesn't work
- Check Vcc_TP and VccRF_TP: Steady 3.3V
- Alternate between Out A and Out B: Doesn't work
- Switch from 100MHz to 125MHz input clock: Doesn't work
Here are some other details:
- Supply: 3.3V 600mA CV with OVP and OCP via a makeshift SMA power cable
- Load: tinySA Ultra Spectrum Analyzer (single ended)
Please provide me with a solution to fix this issue and get my setup back to working condition.
Thanks in Advance!