Part Number: LMX1204
I need a little help clarifying the use of the SYSREF Global Delay in Repeater mode. Based on my interpretation of the data sheet, I should be able to use the delay in repeater mode. The data sheet recommends that SYSREF_DELAY_BYPASS should be in Bypass mode when operating in Repeater mode, but it's not clear why. Later in the data sheet, section 6.3.6.3.2.2 discusses how to use the delay gen in Repeater mode.
Assuming I can use delays in Repeater mode by making sure the STSREF_DELAY_BYPASS is set = 2 (engage in all modes), TICS Pro isn't clear this is correct. On the Main page, when Repeater mode is selected, the SYSREF Global Delay section goes grey as if its not usable. I can't set the SYSREF_DELAY_BYPASS = 2 on the main page as there is only a toggle box that sets it to 0 or 1. I can set it using the User Control page or the Raw Register page, but the SYSREF global delay and individual channel IQ selection are still greyed out.
This is a snap shot of the main page with Repeater mode and SYSREF_DELAY_BYPASS = 2. I can change the values in the grey boxes, but I'm confused why they are grey in this mode. Am I misunderstanding something about possible configurations?