Other Parts Discussed in Thread: LMK61PD0A2, USB2ANY,
I am using an Arty-A7 FPGA dev board to send SPI Commands into the LMX2594. When I send my commands I get no response from the device, I have verified the boards operation by programming it with the LMK61PD0A2. I have also tried programming the board using the LMK61PD0A2, verifying the frequency, then connecting the Arty-A7 and sending a reset command, with no response. I have compared timing and have found no issue and also tried using another Arty-A7.
I have also tried booting the PLL using the guide from the data sheet
Reset = 1
Reset = 0
Program Registers
Delay
Program Cal Bit
I probed the SPI busses on the Arty-A7 "Please Note my SPI Data Bus is set to 5V/Div"