Part Number: LMK1C1102
Other Parts Discussed in Thread: SN74AUC1G74
Dear TI E2E,
I have a slightly odd requirement that I have not been able to find an obvious solution to. I wondered if someone had a nice idea how to solve it please!?
I have a very low noise, CMOS, 200MHz clock, that I would like to distribute. I only want to distribute certain edges. For example, I would like to output every 8th edge, so the output would be a single 2.5ns pulse every 8 cycles. The actual use case has a more varied Nth edge requirement.
I can see the LMK1C1102 has a gate/output-enable pin, but the datasheet says there is maximum 5 cycles output enable/disable time (see specs t1G_ON and t1G_OFF). So it wouldn't work, because as I understand it, I'd have to enable, wait 5 cycles for the first edge, disable, wait another 5 cycles. So I'd get 5 cycles outputted. Is my understanding correct?
One other solution I can see, is to use a high speed flip-flop, like SN74AUC1G74. However, TI don't measure additive jitter for logic (ref https://e2e.ti.com/support/logic-group/logic/f/logic-forum/810935/sn74auc2g32-jitter-of-sn74auc-family). I cannot use a part without any jitter guarantees.
Thank you for any suggestions!
Ben