This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5B12204: 100MHz output immediately after power on

Part Number: LMK5B12204


Dear Technical Support Team,

Could you tell me a clock generator that satisfies the following two conditions?

①100MHz and 165.25MHz(CML or HCSL)

②At least 100MHz is output by default or
 Even if it is not possible the first time, it is possible to output 100MHz immediately when the power is turned on for the second time.

For example, LMK5B12204 is integrated EEPROM and seems to set default setting like 100MH CML output.

Is this covered with ① and ②?

If you have any recommend clock generator, please let me know.

https://www.ti.com/clocks-timing/generators/products.html#116=CML%3BHCSL&1498=Catalog&

Best Regards,

ttd