This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: LMX2594 Output Power below 3 GHz

Part Number: LMX2594

The datasheet only has output power across 3 to 15 GHz. What is the output power below 3 GHz?

  • Hi Peter,

    I measured one board, 50Ω pull up, the output power below 3GHz is as follows:

    2GHz                     8.12dBm

    1GHz                     8.9dBm

    500MHz                8.96dBm

    100MHz                8.84dBm

    50MHz                  8.84dBm

    10MHz                  9.03dBm