Part Number: LMX2571
Other Parts Discussed in Thread: LMX2572
Hi,
According to the datasheet, "The switch can also be configured as a 1:2 fanout buffer, providing the signal on both outputs at the same time."
What is the time difference between the two outputs? Are there any regulations?
Since there is only one PLL system, the two outputs appear to have no time difference at all.
When the customer evaluated it, he said, "Not at the same time."
(But I think it is very difficult to measure the difference in time axis, although it depends on the frequency.)
Is it better to use another product to ensure concurrency in time domain?
Since LMX2572 has a Phase Adjustment function,
Should I recommend this?
Best regards,
Hiroshi