Part Number: CDCE913
Hi all
Would you mind if we ask CDCE913?
Could you let us know required time which is from device start operating to output frequency?
1. After power on, device start up <- How much is the time for wait delay?
2. Register setting via I2C <- It depends on I2C speed.(Address range : 0x00~0x1f)
3. After "2", start of outputting frequency <- After register writing, how much is the time for wait delay?
We would like to confirm "1" and "3".
Kind regards,
Hirotaka Matsumoto