For some reason, in my circuit LMK1C1108 is not working with static input (input = HIGH).
- It works fine with a 20MHz clock input (ASCLK1).
- The output doesn't always rise from LOW to HIGH when there is a step input (ASDI1).
In some cases, the output goes HIGH after an additional attempt (the input goes LOW and is set back HIGH).
- On the one hand, the DS shows a logic-level table and it looks like static input should be supported.
- On the other hand, the DS specifies the output enable/disable time in cycles of the input signal, meaning that the input can't be static.