Part Number: TLC555
Other Parts Discussed in Thread: SN74LVC1G123
Hi,
Can the TLC555 be used in monostable mode with an output pulse duration of 0.5us?
Is there a minimum limit for the duration time?
If it is not available for use in 0.5us, are there any other part numbers that are usable?
Figure 11 in the datasheet shows a duration time range of 1us to 10s.
To achieve a duration of 0.5us, for example, a capacitor of 0.001uF and a resistor of 0.5kohm can be used, but this falls slightly off the chart.
Regards,
Kei