When powering down OUT4, it appears that OUT0 also powers down. This is separate from the voltage enable setting in TICS Pro. When selecting OUT4 as powered down, TICS Pro does not indicate that OUT0 is also powered down. There appears to be a setting we are missing and during testing, we found that shutting down OUT4 also shut down the main 50MHz OUT0 we were using.
I need to document this to ensure that we do not run into this issue in the future as we plan to only use 2 or 3 of the outputs (in addition to OUT0). Can I get confirmation that this behavior is expected? There appears to be no documentation in the datasheet that indicates power to OUT4 is also tied to OUT0.