Part Number: NE555
Other Parts Discussed in Thread: TLC555-Q1
Hi Team,
Are there any timer IC qualified by AECQ100 that meets following requirement?
[Requirement]
keep Hi output for "adjustable time" triggered by input edge.

Regards,
Kai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kai,
The TLC555-Q1 is qualified to AECQ100 and should provide the behavior you're looking for. Regarding the adjustable output length, what are the timing requirements (minimum and maximum output pulse duration)?
However, the trigger input is level sensitive and active low, as opposed to edge sensitive and active high. From your diagram, the level trigger shouldn't be an issue.
To achieve your design requirements using the TLC555-Q1:
The input signal would need to be inverted using a logic inverter. (Like the SN74LVC1GU04)

Regards,
Alex