Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: CDCI6214, CDCE6214, LMK05318B
Hi,
I wish to replace the CDCI6214 to CDCE6214.
In TICS Pro. The CDCI6214 can set the LVCMOS output to CMOSP, CMOSN, and CMOSPN. Then it alos can set to P+ N+, P+ N-, P- N+, P- N-. what does these mean? I think the P+ N+ are the polarities. so i don't understand the CMOSP, CMON, and CMOPN configuration.
About the CDCE6214, the software can only set output to CMOSP, CMOSN, CMOSPN. How to set the polarity? the datasheet show register R59[12], R75[12] and R59[11], R75[11] control the polarity. how to do it in the software? If the CMOSP/N is the polarity, so what is the P+ N+ in CDCI6214 configuration?
CDCI6214 configuration:

CDCE6214 configuration:

One more question: Both CDCI6214 and CDCE6214 has external synchronization function. It can use ch{x}_sync_delay to achieve a fixed delay up to 32 cycles.
1. what is the cycle frequency? the VCO frequency?
2. if i make the sync dealy to 10 cycles. Is that mean the delay between SYNC pin rising edge to outputs first edge is 10 cycles?
3. how to set it in CDCE6214 configuration page. i can find sync function and delay in CDCI6214 configuration page. not in CDCE6214.
Best Regards,
Shu