Part Number: LMK1D1204
Hi,
I'm wondering if it's possible to use a single ended AC-coupled input with a pk-pk voltage of about 0.6V to interface to the input of the LMK1D1204? I would be biasing the IN0_N pin to the recommended halfway voltage of 0.3V, but I'm wondering that if the positive input is AC coupled, do I also need to provide a bias to the positive signal?