This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820: PLL Doesn't Respond to Serial Commands

Part Number: LMX2820
Other Parts Discussed in Thread: USB2ANY, MSP-EXP430FR6989, LMX2594

Hi,

I'm using the LMX2820EVM, and testing with two different setups:

Setup 1: TICS Pro / USB2ANY / LMX2820EVM

Setup 2: MSP-EXP430FR6989 w/ custom SW / LMX2820EVM

I cannot get the PLL to respond to any commands when using Setup 2.

For example, on power-on, if I trigger a calibration via TICS I can measure the SPI bus:

And I see a perfect spectrum at 5.65GHz.

When I try to do the same with Setup 2, I don't get any response from the PLL, and there is no spectrum. Here is the bus capture:

I'm failing to see the difference between these to sequences.

Moreover, when I perform the recommended startup sequence from the LMX2594 datasheet:

Nothing happens on the PLL either, and there is no output. Here's a snippet from the first few bytes of the default sequence:

Perhaps there are some other things I can check and/or am missing?

Thanks.