This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: Inquiry about device configuration

Guru 12775 points

Part Number: CDCE62005

Hello,

The customer attempted to create the configuration below using the CDCE62005 GUI, but an error occurred.

   - AUX IN : 25MHz

   - Output 0 : 100MHz / Output 2 : 66.667MHz / Output 3 : 100MHz

Below is the error message.

Please let us know the cause of the error and the solution.

Thank you.

JH