This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: Phase Noise

Part Number: LMX2595

Hello TI experts, Hi Noel

We want to use the LMX2595 with a 200MHz clock to generate chirp patterns at 19GHz.

For now, we want to test phase noise with the LMX2595EVM, and therefore changed the input frequency to 100MHz.
We use the following settings:

The aim is to get at 100kHz offset a level of -102dB or better.
With this set up, I measure -95.5dB at 100kHz.
Is there a way to reach the goal, besides changing Fpd?

Best Regards
Adrian