This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: LMX-MultiDevice-Outputs-PhaseAlignment

Part Number: LMX2594
Other Parts Discussed in Thread: LMK04832

I'm using the #1Nos LMK04828B and #2Nos LMX2594RHAR in my design to provide #4Nos phase aligned sampling clocks from LMX to my device.

 

I referred some EVK and mapped the LMK to LMX as shown in the attachment. And i have some queries for the same,

 

1- If we are providing the phase aligned clocks from LMK (DCLK_OUT0 and DCLK_OUT4 with same length) to LMX-1 and LMX2, all LMX-1 and LMX-2 output clocks will be phase aligned?

 

2- What is the use of LMX-Sync pin? The Sync pin use is must for LMX output clocks phase alignment if we are using multiple LMX devices?

 

3- In my reference design, the both SDCLK_OUT are configured in LMK as LVDS and only connecting the 'P' of the output clock to the LMX-Sync pin through 0.1uF Capacitor. This is correct? or do you have any recommendation? ( FYI, both LMK and LMX are powered with 3.3V)