Hello,
also in my application the IC power supply is 3.3V and I would like to pull the RSTn pin to +5V.
The datasheet reports that the "input voltage at any pin" must be less than VDD+0.3V and it seems to include also the RSTn pin (even if it is an open-drain output).
Are we really sure that there is no issue if RSTn is pulled to 5V while VDD is only 3.3V?
Best regards,
Angelo