Part Number: TLC556
Other Parts Discussed in Thread: NE555, CD4069UB
I am attempting to setup the TLC556 duel timer to control both frequency and Pulse Width of the output frequency. I have set up the first stage in Astable operation to generate a period of 600seconds (10 min) and the second stage in monostable operation to use a potentiometer to adjust the Ton. I have followed the equations in the datasheet to to setup the output period of the first stage:
Toff = ln(2) * Rb * Ct
300s = ln(2) * Rb * 680uF
Rb = 634k
Ton = ln(2) * (Ra+Rb) * Ct
300s = ln(2) * (Ra + 634k) * 680uF
Ra = 2.49k
When I simulate this circuit using an NE555 timer in LTSpice I get what I expect, a 600 second period with a 50% duty cycle. Thus I created a custom PCB and assembled the components, however when I power it up (12VDC supply) and watch the output with my oscilloscope I get Ton = 644s and Toff = 346s Changing the Resistor values around does effect the Ton and Toff values, so I suspect it's operating just fine but somehow the calculations are not correct? However, that doesn't explain why the simulation would be so spot on and the real hardware would be so off. Attached is my circuit.