Part Number: CDC7005
Hi everyone,
I'm considering using a reference clock oscillator (possibly quartz) at 10MHz and utilizing the CDC7005 synthesizer to generate 5 different ouput frequencies higher than the input frequency. Is this achievable?
I have a query regarding the datasheet of the CDC7005 class product, particularly concerning the output frequencies.
Although it's not explicitly stated in the datasheet, can anyone confirm if the 5 frequencies outputs of the component are independent and can be controlled to generate different frequencies?
Additionally, in the datasheet, there's information about : "Each Output Frequency Is Selectable By x1, /2, /4, /8, /16". Does this imply that we can multiply the input frequencies by 1, 2, 4, 8, or 16? The fact that only frequency
division is mentioned leaves me wondering.
Thank you in advance for your response.