Hello,
In my application, I have a clock with significant jitter. I need to double this clock and filter the jitter. I am currently prototyping on the LMK03328EVM development kit.
With my current settings, the LMK03328 provides a proper jitter clean clock output.
However, I am struggling to have a startup time as indicated by the datasheet §12.2.
PLLx_LOOP BW is set to 1, PLL CL wait is set to 300 ms and PLL1 VCO wait is set to 0.4 ms. R12.1 is set to 1 (parallel calibration of both PLLs). No crystal is used.
From equation 5 or 7 I'd expect the PLL startup time to be 0 (TXO) + 300 ms (TCal) + 0.4 ms (TVco) + 20 ms (Tlock ~ 4/LBW; LBW = 200 Hz), in total 320.4 ms.
However, when measuring from a soft reset till PLL LOL de-asserted, I measure at least 1.8 seconds. This is when a VCO around 4900 MHz is selected, for higher VCO it takes even longer.
Input clock is already available and stable at the time of soft reset.
Are there any points of attention to reduce this startup time? I have already provided the TICS Pro .tcs file in attachment.
Thank you for your support!