Hi,
We are seeing an issue with the LMX2592 PLL. When we change the output frequency from 2.451GHz to 2.551GHz, and then back to 2.451GHz, the PLL loses lock. We initially thought this was an issue with writing to REG30, and to the VTUNE_ADJ register, which got added in a newer version of the datasheet. We removed any writes to the VTUNE_ADJ bits in REG30, and the problem seemed to dissapear, but we are now discovering an intermittent fault on a board with this again. Our code originally did no writes to the VTUNE_ADJ bits, but since this was recently added to the datasheet, this got added in to our interface code.
We are wondering, if A : does VTUNE_ADJ need to be set on temperature dependent scenarios?
and B : does VTUNE_ADJ need to be written in a specific order, i.e do other registers need to be set up beforehand?
Many Thanks,
James