Part Number: LMX2571
Other Parts Discussed in Thread: SN74LVC2G14
I have noticed in the datasheet of 2015, page 11 following points to remember:
When using the Multiplier (MULT > 1), there are some points to remember:
• The Multiplier must be greater than the Pre-divider.
• Crystal mode must be disabled (XTAL_EN=0).
• Using the multiplier may add noise, especially for multiplier values greater than 6.
Question: Is it really not possible, to use the multiplier when an external X-tal is used? What is the reason, as the block diagramm doen't give enough details.
If this is true, how is then the follwing figure 60 to interpret?

I see, that with the LVPECL and the Crystal, the close in phase noise is lower. Is the main reason of the lower phase noise with the Crystal because of the missing muliplier (MULT)?
I'm looking forward to receive from you the proper explanation - many thanks in advance.
Thanks and best regards,
Hanspeter