Other Parts Discussed in Thread: CDCE62005
Hi,
I'm using CDCE62005 in my design to provide clock to some main chips on the board. I wanna use the AUXIN pin with a 25MHz crystal connected and left the SECREF, PRIREF pin unconnected. The output frequency I want is 50MHz,100MHz and 250MHz.
But I've looked through the datasheet of CDCE62005 and I am confused. The internal blocks of CDCE62005 are all dividers. Can I get the frequencies above by setting these dividers? Or are there some multiple frequency block in the CDCE62005?
Last but not the least, what's the relationship between internal VCO and the 25MHz crystal which connected to the AUXIN pin? And what's the function of internal VCO?
Thank you all
Nick