Part Number: LMK04832
Hi all,
I am looking into the LMK04832 for a customer application. The customer plans on feeding in a 3.3V CMOS VCXO input which has a 2.64V minimum pk-pk AC voltage, which appears to be above the maximum spec for the clock single-ended input voltage. Their setup is similar to the one shown in Figure 24 of the datasheet except they do not have a 50ohm termination resistor.
My questions are as follows:
1. Is there an absolute max for the AC coupled single input above 2.4Vpp?
2. Are there are any consequences for running a 2.64Vpp CMOS signal into the LMK04832? Is there any potential damage to the device for doing so?
Thank you for your consideration,
Filipe Rubinstein