This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: noise problem

ss

  • Hi Sam,

    phase noise increase at 7500MHz because it is a fractional channel with very large randomization configuration. That is, PLL_DEN is a very big number and is not an integer multiple of fosc. If you set PLL_DEN to, say, 100000000, phase noise should be good. However, if you set PLL_DEN to 100000001, then phase noise will be bad again.

    when you change frequency, you don't need to program R0 to disable FCAL_EN.