Part Number: LMX2594
Tool/software:
I want to have a 4.0GHz clock output from RFOUTA.
How long will the VCO Calibration time be when the input signal is varying 100KHz with respect to the desired clock, such as 3.9GHz or 4.1GHz?
Feature 1 of the LMX2594 datasheet states "< 20-µs VCO calibration speed".
In Figure 12, it takes roughly 30us to calibrate from 3.7177GHz to 6.9991GHz, and in Figure 13 it takes 10us to 25us to calibrate from 3.4745GHz to 7.0382GHz.
What I want to know is not the large frequency changes shown in these figures.
I want to know how much calibration time is required for small frequency changes at the 100KHz level.