This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

13Mhz sine -> 52Mhz square

Other Parts Discussed in Thread: CDCVF25084, CDC3RL02

Hi,

I have a clock source, 13Mhz, 0.5Vrms, sine wave and want to bring that to 52Mhz, 1.0--4.0Vpp, square wave.

I startet looking at CDCVF25084.

This is fine, but since the output of the CDCVF25084 is sine i have to convert that to square.

So, I am searching for either

  • a component that takes the input of the CDCVF25084 and outputs a square wave

or

  • a component that takes a 13Mhz sine wave input and outputs a 52Mhz square wave

Any suggestions welcome.

Thanks in advance.

Kind regards,

-Alex