Part Number: PLLATINUMSIM-SW
Other Parts Discussed in Thread: LMX2491
Tool/software:
Hello, I have installed the latest version of PLLatinum Sim release (1.6.6.0), and I encounter this error :

From what I understand, this error has occured multiple times to other users in the past, according to both those threads :
In both cases, it was related to the conversion between the way English and French deal with decimals ("1.5" in English, "1,5" in French).
According to those threads, a fix was provided in release 1.6.1, but seemed to have reappeared in 1.6.2.0.
What can be done to fix this issue ? I need to use the software to set-up a filter for the LMX2491 PLL. Is this device supported in other versions of the software that do not feature that EN-->FR bug ? If so, which one, and how can I download it ?
Thank you.
Best regards,
MM