Part Number: LMX25412380EVAL
Other Parts Discussed in Thread: LMX2541, LMX2572LP
Tool/software:
Dear Team,
I would like to generate the local oscillator signal to down-convert my RF signal to a baseband signal. My input frequency range is a maximum of 80 MHz coming out from my ADC. I would like to generate the tunable output frequency and must be in phase with the reference signal. My system requires an output frequency range of 30 MHz to 800 MHz. We are flexible with the frequency resolution, for example, it can be 100 kHz or 200 kHz. However, the IC must contain all the required parts of the PLL integrated internally. In the process, I found the LMX2541 integrated all the components internally. Could you please provide some of your insights regarding my system's specifications? Will the LMX2541 support the reference clock signal from my ADC? I also would like to know about programming the dividers to adjust the output frequency. Is it achievable through the code loader from TI? It is always convenient with other alternatives as well, which you suggest. In the evaluation board of LMX2541, a few components are mentioned as open. Is it adviseable to neglect the components kept open? My concern is about the input, and output frequencies, phase noise to be below as low as possible, very less spurious, and programming the dividers. Could you please also provide the updated schematic for the evaluation board? Thank you in advance.
Kind Regards,
Uday Kiran.