Tool/software:
Hello,
we are using the LMK04832 together with other devices on a 4-wire SPI BUS.
As MISO / serial data out of the LMK04832 we use RESET/GPO. This is shared with MISO pins of other devices.
According the datasheet of the LMK04832, by changing the RESET_TYPE in Register 0x14A the behavior of this pin can be changed.
Here it is decribed that the pin can not be set to high impedance.
When using RESET_TYPE= 6 (0x06) Output (open-drain) the output pulls to LOW level. This did not help us.
We were interested to see how the pin behaves when using RESET_TYPE=5(0x05) or 7(0x07)
To our pleasant surprise, with RESET_TYPE=7(0x07) the output appears to be high impedance.
Could you please doublecheck and confirm this?
This would be very helpful.
Thank you and best regards
Christoph