Part Number: LMK01000
Tool/software:
Hi
I consider using the LMK01000 for JESD204 fanout buffer and SYSREF divider.
input clock 120MHz
output clocks 120MHz:
------------------------------
2 x LVPECL
2x LVDS
output clocks SYSREF - 8MHz with delay adjustment
---------------------------------------------------------------------
1 x LVPECL
1 X LVDS
it is stated that "Clock output delay registers (CLKoutX_DLY) support a 150 ps step size and range from 0 to 2250 ps of total delay"
is the 150ps is relevant also for 120MHz input?
any relation between the clock input period to the delay adjustment?
please advise
best regards
shay