Part Number: CDCE6214
Tool/software:
Hi Team,
Some questions while designing with CDCE6214.
Output clocks are 1MHz, 2MHz, and 40MHz
The input clock can be from a 25MHz crystal or from a 25MHz TCXO.
The schematics as below and the questions are:
CLOCK_GENERATOR_TI_CDCE6214_SCHEMATIC1 _ PAGE1.pdf
1. Can this chip be controlled to start synchronously on all 3 outputs?
2. Can this chip to be controlled with a enable-input-pin to start all 3 clocks at the same time?
3. Can any I/O pin be used to function as an “Enable-pin”
Thanks.