This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820EVM: Clarification for no alteration for previous design

Genius 17815 points
Part Number: LMX2820EVM
Other Parts Discussed in Thread: LMX2487E

Tool/software:

Hi Experts,

We received query about the operation of this unit - LMX2820EVM.

I have a stable 100MHz OCXO that I plan on using for the OSC input. My research group currently operates an LMX2487E for producing a 3.417GHz frequency, and we had to replace the onboard VCO with a custom one to achieve this. I wanted to be sure no alterations need to be made on the board to produce the frequency range of the board.

Further, I would like to clarify the use of the RFIN of the unit. That's used to phase lock an external VCO to the OSC input, and reduce the N to improve the phase noise, correct? 

Thank you.

Regards,
Archie A.

  • Hi Archie, 
    You can leave the EVM as is for quick evaluation but on your own board please use PLLatinumSim to calculate optimal loop filter values for your application. 

    Further, I would like to clarify the use of the RFIN of the unit. That's used to phase lock an external VCO to the OSC input, and reduce the N to improve the phase noise, correct? 

    That is correct - RFIN pin can be used for external VCO mode. 

    Regards, 

    Vicente